HomeHomeGeneral Categor...General Categor...Simulation Tool...Simulation Tool...DC to DC Designer websiteDC to DC Designer website
Previous
 
Next
New Post
11/9/2015 8:07 AM
 
Mike,

Our IT department has fixed the issue - let me know if you have any trouble accessing the tool now.

Thanks,
David
 
New Post
11/9/2015 9:03 AM
 

Hi David,

The website is back up but the tool is no longer behaving the same as it was several weeks ago. I am running a case for the MP2162 and I change the RFB2 from 200K (default) to 187K. When I click on “Recalculate Compensation” it changes RFB1 from 200K to 165K but it also changes the RFB2 that I changed to 187K back to 200K. I have the “Manually Change Power Stage?” checkbox checked. It did not behave this way before. Previously the tool reported a value for RFB1 of 154K when I set RFB2 to 187K. Also the waveform amplitude is 0 to 3.3V even though I set my output voltage to be 1.1V.

 
Previous
 
Next
HomeHomeGeneral Categor...General Categor...Simulation Tool...Simulation Tool...DC to DC Designer websiteDC to DC Designer website