HomeHomeGeneral Categor...General Categor...General Technic...General Technic...MPS2637 reverse batteryMPS2637 reverse battery
Previous
 
Next
New Post
3/1/2017 3:12 AM
 

We have design for using a battery socket with a 2.6Ah 18650 format cell. Unfortunately, the 18650 batteries can be reversed in socket (that is + instead of -). The problem is that some cylindrical batteries do have internal protections, others (especially ultra low cost, un-branded) don't.

 

So the customer can insert battery in wrong polarity and more dangerous, potentially can use a no-name battery without any kind of protection.

 

Our idea is to use a fuse in series with battery (glass, smd, 30mR) and a reverse polarized diode in parallel with battery in such way that if normal connection, nothing happens. Will be a little voltage loss across fuse so no more 4V2 when charging with high currents. In case of wrong polarity, fuse will blow which will make the module out of service. PPTCs have much more resistance and moreover, resistance will increase with trips.

 

MPS2637 is internally protected to reverse battery?

Other ides for protecting in such situations?

 

Thank you,

 
New Post
3/1/2017 10:26 AM
 

Hi Jimy,

 

MP2637 has Internal Battery Reverse Leakage Blocking feature. There no need to have external fuse for reverse battery protection.

 

Thanks,

Kevin

 
Previous
 
Next
HomeHomeGeneral Categor...General Categor...General Technic...General Technic...MPS2637 reverse batteryMPS2637 reverse battery